Skip to main content
cn2
Associate
March 21, 2017
Question

LSM6DSL Min/Max specifications for ODR (Output Data Rate)

Posted on March 21, 2017 at 15:35

I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as 'Typical'. Could I get a more precise specification for the ODR, e.g. min/max values over the entire temperature range. I suppose this ODR is generated from an internal oscillator with tolerance, temperature drift, ...

    This topic has been closed for replies.

    1 reply

    ST Employee
    April 9, 2017
    Posted on April 09, 2017 at 09:02

    Unfortunately this information cannot be shared on ST Community web.