Visitor II
July 21, 2020
Question
LSM6DSL is used on mtk8735 platform (Android) which Accel XYZ data fulll-scale is wrong throuh low-pass filter.
- 1 reply
- 874 views
HI, We used lsm6dsl sensor on mtk8735 platform (Android). We found that the low-pass filter is used in the high-frequency working mode which freq is greater than 26hz. the XYZ direction data range which obtained is not within +-4G, but 0x10h register value is 0x48 which ODR is LSM6DSL_REG_CTRL1_XL_ODR_104HZ and full-scale with +-4G.
We kept turning the device and print the original value of accelerometer XYZ. We saw that the data is ranged in + - 1g which is abnormal as normal.
we found tha sensor data is right only the ODR bellow LSM6DSL_REG_CTRL1_XL_ODR_26HZ without low-pass filter.Please give us a reasonable explanation and look forward to your reply. thanks