Skip to main content
Avdhoot
Visitor II
Feb 11, 2019 12:19 PM UTC
Question

LSM6DSL

Hello,

I'm planning on using the LSM6DSL in my design.

For the same reason I have bought & worked on evaluation board, STEVAL-MKI178V1 .

In the documentation of this board, I have found that pin no. 10 & pin no. 11 both are used & connected.

But in LSM6DSL datasheet these pins are shown as NC pins.

I'm getting the data using evaluation board, but unable to get the data using IC only.

I'm using nordic processor & through I2C communication I'm reading the accelerometer & gyro values.

Do I need to connect pin no. 10 & 11 in hardware?

This topic has been closed for replies.