Skip to main content
Visitor II
Feb 19, 2025 10:58 AM UTC
Solved

LSM6ds3tr Pin Connection with Microcontroller

Hello 

To receive various Interrupt events how INT1 and INT2 Pins of LSM6ds3tr need to be connected with Microcontroller ?

My assumption is INT1 and INT2 pins need to be connected with microcontroller GPIO pins and GPIO pins has to be configured to catch IMU Interrupt events. Please Support whether this assumption is correct or not.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 20, 2025 10:20 AM UTC

Welcome @Ajit1, to the community!

Yes, your assumption is correct: in order to trigger an interrupt, INT1 and/or INT2 must be connected to interrupt-capable GPIOs.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 20, 2025 10:20 AM UTC

Welcome @Ajit1, to the community!

Yes, your assumption is correct: in order to trigger an interrupt, INT1 and/or INT2 must be connected to interrupt-capable GPIOs.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.