Skip to main content
prachi
Visitor II
November 23, 2016
Question

LSM6DS33 supply voltage

Posted on November 23, 2016 at 11:58

Hi,

The typical supply voltage for the LSM6DS33 is 1.8V and the maximum limit is 3.6V. Is it fine if a supply voltage of 3.3V is continously provided to the device?

Regards,

Prachi 

#lsm6ds33
This topic has been closed for replies.

1 reply

Petr S
ST Employee
December 1, 2016
Posted on December 01, 2016 at 12:14

Hello,

Yes, since the LSM6DS33 analog supply voltage range is from 1.71 V to 3.6 V it is more than fine if a 3.3V supply voltage is continuously provided to the device.

Thank you and best regards,

Petr