Skip to main content
Alex Dim
Associate II
December 12, 2018
Question

LSM6DS3 sensor hub

Hello,

i read the AN4650 application note for the LSM6DS3 accle+gyro and i tried to implement the sensor hub routine with a MAG3110, like the one in the examples but it doesn't seem to work, is there another application note or a sample code that i can look at?

Thank you in advance,

Alex

    This topic has been closed for replies.

    3 replies

    ST Employee
    December 12, 2018

    I doubt the problem is in our application note, anyway you can find an example in ST GiHub:

    https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm6ds3_STdC/example

    Alex Dim
    Alex DimAuthor
    Associate II
    January 29, 2019

    Hello,

    i studied extensively the "sensor_hub_lis2mdl_lps22hb_no_fifo_simple" example so i can use the LSM6DS3 with an external magnetometer. There are 4 lines that i cannot understand, in the main example there is the code below

     /*
     * Configure LIS2MDL on the I2C master line
     */
     
     lis2mdl_operating_mode_set(&mag_ctx, LIS2MDL_CONTINUOUS_MODE);
     lis2mdl_offset_temp_comp_set(&mag_ctx, PROPERTY_ENABLE);
     lis2mdl_block_data_update_set(&mag_ctx, PROPERTY_ENABLE);
     lis2mdl_data_rate_set(&mag_ctx, LIS2MDL_ODR_50Hz);

    that passes all the desirable options to the registers of the external LIS2MDL magnetometer, i cannot understand how this is possible since it doesn't use the sensor-hub pass-through feature or the required steps to write to an external slave sensor.

    Thank you in advance, you have been very helpful

    •  

    Alex Dim
    Alex DimAuthor
    Associate II
    December 12, 2018

    Thank you, i will study that and see what i did wrong.