Skip to main content
darla14
Associate III
September 19, 2014
Question

LSM6DS0 6 AXIS Sensor Query

Posted on September 19, 2014 at 08:04

Hi,

I am writing code for LSM6DS0 module.I could not find any reference driver or Initial setting needs to be done .

In the datasheet there are two modes : 

(1) Accelerometer active and Gyro Inactive

(2) Accelerometer active and Gyro active

Is there no way to power down both.

As a thumb rule I will set the ODR and enable the Power ON mode.Apart from this is there any special settings needs to be done like BDU,HP filters,FIFO, etc for this module.

Initially I just aim to read the sensor data of Accelerometer and Gyroscopes andlookign for minimal settings to be done.

Any special settings needs to be done.

Please suggest.

rgds,

R

#lsm6ds0 #gyroscopes #accelerometer
This topic has been closed for replies.