Skip to main content
don2399
Visitor II
January 11, 2013
Question

LSM330LDC SPI mode

Posted on January 11, 2013 at 18:05

Section 6.2 of the data sheet says that ''SPC,SDI,SDO are common'' however there are 2 different SDO pins, SDO_A and SDO_G. Has anyone tried connecting the two SDO pins on the target board? 

Does anyone know if I2C mode always active when the CSx pin is HI? If so how do you prevent the I2C module for erroneously receiving a command from other devices that may be operating on the SPI bus?

Thanks
    This topic has been closed for replies.

    3 replies

    Gerardo GALLUCCI
    ST Employee
    May 27, 2013
    Posted on May 27, 2013 at 16:22

    Any update?

    IHS1
    Associate II
    June 6, 2013
    Posted on June 06, 2013 at 09:50

    Hi

    I have the same

    doubt, the

    datasheet

    is confusing

    on this issue.

    Furthermore

    evaluation

    board

    STEVAL

    -

    MKI109V2

    and

    ''Unico

    GUI''

    using

    I2C

    protocol

    .

    Best regards

    theparitt
    Associate III
    February 20, 2015
    Posted on February 20, 2015 at 18:40

    agree. so confusing. i am not sure that it is possible that i connect two SDO line together since i enable / disable  Accere/Gyro and Magnet seperately.