Skip to main content
vahramhambardzumyan
Visitor II
January 28, 2016
Question

LSM330DLC I2C

Posted on January 28, 2016 at 13:10

Dear All,

I am using LSM330DLC gyro-acc on my board and I have forgotten place pull-up resistors on the SPI/I2C selection pins. However it works fine. My question is can I develop my project without these pull-up resistors?

It is mentioned, in datasheet, these pins must be high for I2C operation, but in my case it is 0V and I2C works well.

This topic has been closed for replies.

1 reply

louda.marian
ST Employee
July 1, 2016
Posted on July 01, 2016 at 15:37

Hello,

You are lucky man that it works fine. These pins should be high for I2C communication. To left these pins unconnected is a problem.

Best Regards,

Marian