Skip to main content
Gary Sugar
Visitor II
April 2, 2018
Question

LSM303DLHCTR - Peak Current Consumption Issue

Posted on April 02, 2018 at 19:18

I'm using an LSM303DLHCTR in an application where I'm reading its X, Y and Z magnetometer values once per 20 ms, and have noticed that the chip seems to consume 10 mA or more of current from its 3.3V supply (VDD pin) - for a short interval of about 4 ms during each 20 ms cycle - presumably while it's doing a magnetometer ADC conversion. The 10 mA is much higher than I expected, since the data sheet says to expect only 110 microamps of current draw. Accelerometer is disabled in my application. 

Has anyone else seen this behavior? 

This topic has been closed for replies.

1 reply

ST Employee
April 4, 2018
Posted on April 04, 2018 at 16:15

Yes, there are peaks on the Icc, they are typical for magnetometer operation.

The value 110uA written in datasheet is average value.