Skip to main content
adam239955
Associate III
July 10, 2015
Question

LSM303DLHC DRDY signal

Posted on July 10, 2015 at 17:34

LSM303DLHC Data Sheet says

The LSM303DLHC features two data-ready signals (RDY) which indicate when a new set of measured acceleration data and magnetic data are available

but Figure 4 only shows one DRDY pin out, does that mean that when the pin is set, both accelerometer and compass has new data, or do I have to check status/ctrl registers to see if accelerometer or magnetometer has data? #lsm303dlhc #drdy
This topic has been closed for replies.