Skip to main content
feverest
Visitor II
June 10, 2014
Question

LSM303D Noise levels?

Posted on June 10, 2014 at 12:58

I am using an LSM303D and find the noise level surprisingly high. I have configured it with the following parameters:

#define CTRL0 0b00000000 //for normal mode, filters by-passed

#define CTRL1 0b00011111 //update after read, and all axes of acceleration enabled at 3.125Hz

#define CTRL2 0b11000001 //50Hz anti-alias, +/- 2g, no self-test, (SPI 3-wire)

#define CTRL3 0b00000000 //No INT1 actions

#define CTRL4 0b00000000 //No activity on INT2.

#define CTRL5 0b01100000 //No temperature, high-res magnetic, 25Hz, no INT2 latching

#define CTRL6 0b00000000 //+/-2gauss sensitivity.

#define CTRL7 0b00000000 //normal acceleration filter, no Temp, magnetic always on, continuous conversion mode

I have it at a fixed position and static magnetic field and get the values shown in the attached XLSX file:

Could I improve it?

This topic has been closed for replies.

1 reply

zhangyangpz0806
Visitor II
June 20, 2014
Posted on June 20, 2014 at 10:07

Hi,frank,how is it going?