Skip to main content
Eetu Nevalainen
Associate II
June 27, 2019
Question

LSM303AH self-test fails

Hi,

We're not able pass LSM303AH accelerometer self-test on our products. Please see one of the results below. The datasheet doesn't describe what may be wrong if the self-test fails so could you guide us with this issue.

As far I understand the allowed difference on LSM30AH is: 70 <= |st avg - nost avg| <= 1500.

nost x: {56, 76, 68, 84, -40}, avg: 48.8

nost y: {-180, -172, -220, -148, -204}, avg: -184.8

nost z: {-8284, -8284, -8296, -8284, -8284}, avg: -8286.4

st x: {3116, 3128, 3240, 3228, 3164}, avg: 3175.2

st y: {2460, 2460, 2504, 2468, 2488}, avg: 2476

st z: {-5588, -5608, -5596, -5588, -5588}, avg: -5593.6

x diff: 3126.4

y diff: 2660.8

z diff: 2692.8

// Eetu

This topic has been closed for replies.

8 replies

Eleon BORLINI
ST Employee
June 28, 2019

hi @Eetu Nevalainen​ , which FS did you set? Please note that these values are for 2g. And did you write 01h to ST [2:1] of CTRL3_A to enable positive self test? Regards

Eetu Nevalainen
Associate II
June 28, 2019

FS is set to 4g and positive self-test is enabled. Here's I2C traces from the self-test procedure. I didn't notice anything out of ordinary but maybe you can spot something.

Eleon BORLINI
ST Employee
June 28, 2019

​if FS is 4g you have to double the self test limits (the ds ones refers to FS 2g), changing from min 70mg, max 1.5g to min 140mg, max 3g. In this way, y and z values falls inside the limits, not the x value, which is too high... are you moving the LSM303AH during the self test? Regards

Eleon BORLINI
ST Employee
July 5, 2019

​Hi @Eetu Nevalainen, yes, consider that in normal mode case OUT_X/Y/Z_L/H_A data have to be computed on 16 bits and in two's complement (although the two lsb are 0). Regards