Skip to main content
Selim Sagir
Associate III
February 6, 2024
Solved

LSM303AGR gives weird values output of the accelerometer

Hi,
I am using examples from the github repo to test accelerometer. I can read device id from both accel and magnetometer. Also I can read back the registers I set.  However, when it comes to read accelerometer, I read same values from all axis of the accelerometer such as A0A0A0 or 808080 and so on. Another behavior I observed is sometimes, boot register stuck as 1 after I use to BOOT bit from CTRL_REG5_A.
Also I read very low values from magnetometer and 0 from temperature sensor.
Is there any idea what is going wrong?

Thanks.

This topic has been closed for replies.
Selim Sagir
Selim SagirBest answer
Associate III
February 7, 2024

Hi @Federica Bossi ,
I think problem is the auto address incrementation for the multiple reads. Because when I've read the axis out registers one by one, I can see correct values. Also when I changed to LSM303AGR_OUT_X_L_A (0x28) to 0xA8, library function (lsm303agr_temperature_raw_get) also gives correct outcomes
Thanks,
Selim.

4 replies

Federica Bossi
ST Technical Moderator
February 7, 2024

Hi @Selim Sagir ,

Have you made any changes to the examples on github or are you using them as they are loaded?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Selim Sagir
Selim SagirAuthorBest answer
Associate III
February 7, 2024

Hi @Federica Bossi ,
I think problem is the auto address incrementation for the multiple reads. Because when I've read the axis out registers one by one, I can see correct values. Also when I changed to LSM303AGR_OUT_X_L_A (0x28) to 0xA8, library function (lsm303agr_temperature_raw_get) also gives correct outcomes
Thanks,
Selim.

Federica Bossi
ST Technical Moderator
February 7, 2024

Hi @Selim Sagir ,

Ok, so have you found how to solve this issue?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.