Skip to main content
Ozone
Principal
Jan 14, 2025 12:27 PM UTC
Question

LSM303 register interface compatibility ...

I recently began working on an driver software for a magnetometer application, which is intended to support both the LSM303 (the LSM303DLHC, to be exact), and the HMC5883L from Honeywell.

And I didn't fail to notice that both devices have identical I2C addresses and identical values for the identification register values (IRA, IRB and IRC).

My question would be, is this intentional ?

Not that it is of utmost importance to me, I found another way to distinguish between both. The HMC5883 has no accelerometer part, and when I can write into a RW accelerometer config register and read the same value back, I deal with a LSM303, else with a HMC5883.

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
Jan 14, 2025 12:39 PM UTC

@Ozone wrote:

My question would be, is this intentional ?


More likely accidental, I should think.

They are devices from two different manufacturers - I doubt the designers from either company go around checking all competitor's parts ...

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
OzoneAuthor
Principal
Jan 14, 2025 3:06 PM UTC

> They are devices from two different manufacturers - I doubt the designers from either company go around checking all competitor's parts ...

That got me wondering.
And not only the I2C adress and ID register values are the same, the internal addresses of those registers as well.
Meaning, you send a I2C read request with the same register offset, and get identical answers from both devices.

I think this is no coincidence, one wanted to be compatible with the other, I guess.
Although I don't expect a full disclosure here ...

Andrew Neil
Super User
Jan 14, 2025 3:15 PM UTC

So are any/all of the other registers compatible, too?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.