Skip to main content
Visitor II
Mar 20, 2026 12:30 PM UTC
Question

LPS28DFW511-LPS28DFWTR

We are currently experiencing issues with the LPS28DFW.
We observe pressure values dropping to 0 or even negative ranges (e.g., around -400 mPa), as well as unexpectedly high values (up to approximately 1200 mPa), while the expected range should be around 950 mPa. We are also seeing abnormal temperature outputs, including unrealistically low values (e.g., around -400°C).

this happens when the sensor is in contact only with air and also when it is in contact only with water. When the sensors from the field they are brought back in the lab the sensors seem to recover on their own and return to normal readings.

1 reply

Federica Bossi
ST Technical Moderator
Mar 27, 2026 10:59 AM UTC

Hi @MBENRiverkin ,

It seems to be an issue with reading and interpreting data from sensor.
Please share your code and the sensor registers settings.

Thanks!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.