LPS22HH temp sensing: Temperature error and sensor-to-sensor spread is LARGER than datasheet specifications.
LPS22HH temp sensing: below 30°C, error exceeds ±1.5°C and sensor-to-sensor spread is large; need causes and solution.
The LPS22HH is used to measure ambient temperature. Below 30 °C, the reported temperature deviates from the reference ambient temperature by more than the specified accuracy of ±1.5 °C, and the sensor-to-sensor output variation is large. Ambient temperature instability and firmware/software implementation issues have been ruled out.
Question
What could be the causes of the out-of-specification temperature error and the large sensor-to-sensor output variation? How to solve it?
Operating Conditions
The sensor is soldered onto the PCB of a mass flow meter and is used to acquire ambient temperature and pressure. The sensor is not covered or enclosed. Ambient temperature is controlled by a temperature chamber and remains within the sensor operating range of -40 °C to +85 °C.
Observed Data
With the ambient temperature set to 0 °C, four sensors report 4.72 °C, 0.91 °C, 5.33 °C, and 2.64 °C, respectively. One sensor reports -3.3 °C at -10 °C and 26.96 °C at 25 °C; its error exceeds the specified limit over this interval. At each measurement, the ambient temperature had already been stable for more than 40 minutes.