Skip to main content
Associate III
Mar 19, 2025 9:59 AM UTC
Solved

LPS22HB Absolute pressure accuracy

Hello,

in the datasheet of LPS22HBTR the absolute pressure accuracy is between 0. and 1 mBar in the range of 0°C and 65°C .

Please have more information about the absolute pressure accuracy in negative temperature ? because i will use it betwen -20°C and 0°C

thanks 

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Mar 21, 2025 8:34 AM UTC

Hi @ljm ,

We can't provide this type of information on ST Community.

If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Mar 21, 2025 8:34 AM UTC

Hi @ljm ,

We can't provide this type of information on ST Community.

If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.