Skip to main content
Associate II
Nov 20, 2024 3:49 PM UTC
Solved

LPS22DF static addresses: 0x6B/0x6A or 0x5C/0x5D

We have a STEVAL-MKI224V1 kit, which should be equipped with a LPS22DF. I have tried to use the static (I2C) address of the sensor, and after much time, I discovered it is (depending on the state of SDO) 0x5C/0x5D, and not 0x6B/0x6A, as stated in the datasheet.

Strangely (or not) 0x5C/0x5D is the static address of the LPS22HH, but according to the GETPID command, I do have a LPS22DF.

Thank you.

This topic has been closed for replies.
tcachatBest answer
Associate II
Nov 28, 2024 8:39 AM UTC

To conclude, the static address is 0x5C/0x5D, which is also the I2C 7-bit address, and the datasheet should be improved (Table 15, SETDASA ...).

3 replies

Federica Bossi
ST Technical Moderator
Nov 22, 2024 7:47 AM UTC

Hi @tcachat ,

Which datasheet version do you have?

If you look at DS13316, in section 7.2.1, you find: 

The 7-bit slave address (SAD) associated to the LPS22DF is 101110xb. The SDO/SA0 pin can be used to modify
the less significant bit of the device address. If the SA0 pin is connected to the voltage supply, LSb is 1 (7-bit
address 1011101b=5Dh), otherwise if the SA0 pin is connected to ground, the LSb value is 0 (7-bit address
1011100b=5Ch). This solution permits connecting and addressing two different LPS22DF devices to the same I²C
lines.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
tcachatAuthor
Associate II
Nov 25, 2024 8:18 AM UTC

I have DS13316 - Rev 2, where I can read the same section 7.2.1 as you, with the true static addresses. But in section 7.4.1, Table 15 shows:

SETDASA     0x87     Assign dynamic address using static address 0x6B/0x6A depending on SDO pin.

Why that???

Moreover searching for the word "static" in the whole datasheet, I find the previous table, but do not section 7.2.1...

tcachatAuthorBest answer
Associate II
Nov 28, 2024 8:39 AM UTC

To conclude, the static address is 0x5C/0x5D, which is also the I2C 7-bit address, and the datasheet should be improved (Table 15, SETDASA ...).