Skip to main content
Associate III
Nov 13, 2023 8:27 AM UTC
Question

LPS22DF OR LPS28DFW

Hello,

I have question please, can you tell me the protection index (IP) of the LPS28DFW ? 

also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i don't find any information on the datasheet about the High shock survivability.

Can you tell me if the 2 sensors have the same High shock survivability or not ? 

Thank you very much 

This topic has been closed for replies.

8 replies

ljmAuthor
Associate III
Nov 10, 2023 10:52 AM UTC

Hello,

I have question please, can you tell me the protection index (IP) of the LPS28DFW ? 

also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i didn't found any information in the datasheet about the High shock survivability.

Can you tell me if the 2 sensors have the same High shock survivability or not ? 

Thank you very much 

Federica Bossi
ST Technical Moderator
Nov 16, 2023 3:44 PM UTC

Hi @ljm ,

If it is not written on the datasheet, there is no IP certification.

By construction and package closure, the 28DFW is more robust than the 22DF and therefore has a higher high shock survivability than 22000g.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ljmAuthor
Associate III
Nov 20, 2023 12:41 PM UTC

thank you very much for your feedback.
from what i've seen the price of the lps28dfw is almost 2 to 3 times more expensive than the lps22df.
is this difference explained by the advantage of the LPS28DFW which has a fairly high measuring range and the added gel for waterproofing ?
One last question please, for the LPS28DFW's dust tightness, can you recommend any of your products that might help me ?  and thank you.

ljmAuthor
Associate III
Nov 17, 2023 12:50 PM UTC

thank you very much for your feedback.
from what i've seen the price of the lps28dfw is almost 2 to 3 times more expensive than the lps22df.
is this difference explained by the advantage of the LPS28DFW which has a fairly high measuring range and the added gel for waterproofing ?
One last question please, for the LPS28DFW's dust tightness, can you recommend any of your products that might help me ?  and thank you.

Federica Bossi
ST Technical Moderator
Nov 22, 2023 9:40 AM UTC

Hi @ljm ,

For dust, LPS28DFW is more immune due to the presence of gels, while dust on LPS22DF could alter the measurement by closing the holes where the pressure is read.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ljmAuthor
Associate III
Nov 22, 2023 12:38 PM UTC

Hi @Federica Bossi 

Thank you for your reply.
Does this mean that the existing gel on the LPS28DFW protects against water and dust at the same time? Because the environment where the sensor is used, there is too much dust? Do you have any idea if the existing gel on the LPS28DFW protects against large dust (in mm) or even for small dust (in micro-meter)?

ljmAuthor
Associate III
Nov 22, 2023 4:01 PM UTC

hello @Federica Bossi 

because as far as I know, dust can accumulate on the gel.