Skip to main content
Associate II
Sep 7, 2025 10:08 AM UTC
Solved

LPF filter on IIS2ICLX inclinometer

I would like to implement a low pass filter to filter out noise at frequencies above 2Hz on the IIS2ICLX inclinometer. I would like to have as high an ODR as possible, let's assume 833Hz. My signal has a low frequency, around 0.5Hz.

LPF1 will clearly not help me - the response is flat out to 100Hz.

To implement the filter using LPF2, would the following register configurations be suitable:

CTRL1_XL :

ODR bits 0b0111 for 833Hx ODR

LPF2_XL_EN bit 0b1 to enable LPF2

CTRL8_XL

HPCF_XL bits 2:0 set to 0b110 for cutoff of ~2Hz (=833Hz ODR / 400)

HP_REF_MODE_XL set to 0b0 to disable HP filter

FASTSETTL_MODE_XL set to 0b0 to disable fast settling mode

HP_SLOPE_XL_EN set to 0b0 to disable slope filter

 

I would be extremely grateful for any help implementing my filter - thanks for reading this far!

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Sep 11, 2025 12:09 PM UTC

Hi @chisatholm ,

Your settings are correct and suitable for implementing a low-pass filter with cutoff ~2 Hz at 833 Hz ODR on the IIS2ICLX.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Sep 11, 2025 12:09 PM UTC

Hi @chisatholm ,

Your settings are correct and suitable for implementing a low-pass filter with cutoff ~2 Hz at 833 Hz ODR on the IIS2ICLX.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.