Skip to main content
JLloy.2
Associate
Mar 4, 2021 12:27 PM UTC
Solved

Looking for MEMS IMU that can measure impact level g's and rotation

I am working on a biomedical research project to study how a head impact, such as in American Football, is transmitted through the brain.

To make this work, I need to embed the smallest IMUs into a synthetic brain. The IMUs need to be able to measure angular motion at 1000-2000 deg/s (no problem) and also be able to measure linear acceleration in the 200 - 400 g range.

After days of searching, I am unable to find any IMUs that meet this criteria.

Does anyone have any ideas??

Thanks, John

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Mar 4, 2021 3:00 PM UTC

    Hi John @JLloy.2​ ,

    I confirm you that the current best trade-off for an IMU with a mid-g accelerometer is the LSM6DSO32.

    The high-g accelerometer (i.e. above 100g) are so far stand-alone products but not so much because the gyro would risk being damaged by those shocks (since IMUs can sustain up to 10.000g shocks), but because the gyro sensitivity will not be accurate at those linear acceleration intensities.

    You could think to combine a stand alone gyro such as the L3GD20H, and a stand alone high-g accelerometer, such as the H3LIS331DLTR.

    Should be the device you are looking for a medical-graded device?

    Anyway, in case ST will introduce a new product with the characteristics you are requiring (it would be useful -but not strictly necessary- to have the related total addressable market and the business volume), we will notify it to you.

    -Eleon

    4 replies

    Ons KOOLI
    Visitor II
    Mar 4, 2021 1:19 PM UTC

    Hi JLIoy.2,

    Please see the iNEMO-Inertial Modules provided by ST.

    I really hope this is helpful.

    Best Regards,

    Ons.

    JLloy.2
    JLloy.2Author
    Associate
    Mar 4, 2021 1:29 PM UTC

    Thank you. The INEMO IMUs would be perfect, but it seems max linear acceleration is only +/- 32g. I need 200-400g, such as the H3LIS331DLTR, combined with a gyro, but cannot find any such product.

    Ons KOOLI
    Visitor II
    Mar 4, 2021 2:07 PM UTC

    Hi JLIoy.2,

    Okay I will report your question about maximum range acceleration and provide you with the answer sooner.

    Best Regards,

    Ons.

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Mar 4, 2021 3:00 PM UTC

    Hi John @JLloy.2​ ,

    I confirm you that the current best trade-off for an IMU with a mid-g accelerometer is the LSM6DSO32.

    The high-g accelerometer (i.e. above 100g) are so far stand-alone products but not so much because the gyro would risk being damaged by those shocks (since IMUs can sustain up to 10.000g shocks), but because the gyro sensitivity will not be accurate at those linear acceleration intensities.

    You could think to combine a stand alone gyro such as the L3GD20H, and a stand alone high-g accelerometer, such as the H3LIS331DLTR.

    Should be the device you are looking for a medical-graded device?

    Anyway, in case ST will introduce a new product with the characteristics you are requiring (it would be useful -but not strictly necessary- to have the related total addressable market and the business volume), we will notify it to you.

    -Eleon