Skip to main content
anna
Associate
November 3, 2016
Question

LISDH12 high consumption

Posted on November 03, 2016 at 17:34

Hi all,

i use an accelerometer  LISDH12, and it have a very high consumption (400 uA).

I have this configuration;

  • SCL/SDA connect to vdd with 4.7k
  • CS to high because i want to use a i2c
  • SDA0 put on ground

Someone have a suggestion about this problem?

Thanks,

Anna

#high-consumption
This topic has been closed for replies.

3 replies

ST Employee
November 4, 2016
Posted on November 04, 2016 at 11:07

I suppose the sensor is LIS2DH12.

You didn’t specify if the sensor is running and what is the ODR, it has an influence on current consumption.

Also connecting SDO/SA0 pint to ground will induce

mailto:~130uA@3.3V

current. So if possible connect the SDO/SA0 pin to Vcc and use the second I2C address.

Best regards

Miroslav

anna
annaAuthor
Associate
November 9, 2016
Posted on November 09, 2016 at 09:57

HI Miroslav,

The sensor is power off. I set the register CTRL_REG1 to 00. So i exspect that the consumption is 0.5 uA.  

Furthermore, if i use a package STEVAL-MKI135V1 on my evaluation board it works correctly, the consumption is ok. But on my prototype is high.

Thanks,

Anna

ST Employee
November 11, 2016
Posted on November 11, 2016 at 11:31

Can you please share your schematic?

Best regards

Miroslav