Skip to main content
TBart.1
Associate II
July 21, 2024
Question

LIS3MDL Temperature problem.

Hello. We know that lis3mdl is temperature sensitive, i.e. there is a scale shift. From what we have read, this cannot be compensated for with software ( Or maybe it's possible? ). Therefore, can this be prevented physically, e.g. by using some thermal paste? The idea is to prevent lis3mdl from heating up too much. Our operating temperature range is 10-35 degrees Celsius. Thanks.

This topic has been closed for replies.

3 replies

AScha.3
Super User
July 21, 2024

Hi,

>The idea is to prevent lis3mdl from heating up too much.

from ds:

AScha3_0-1721559152682.png

The lis3 heating up at 0.6 mW power consumption ? (at its nominal 2.5V supply)

No, never... almost impossible, to get any temp.rise to measure, i think.

btw :   at which voltage you use it ?

If you feel a post has answered your question, please click on " Best Answer ".
TBart.1
TBart.1Author
Associate II
July 21, 2024

It's not about the voltage heating up, it's about the external ambient temperature.

Federica Bossi
ST Technical Moderator
July 22, 2024

Hi @TBart.1 ,

Did you perform some tests? Which is the offset drift you observed?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.