Skip to main content
Nmaje.1
Associate
June 7, 2023
Question

LIS3MDL connected to ISM330dhcx as external sensor is giving NACK after some hours of continous run.

i have a maaxboard that is connected (via i2c) to ism330dhcx. Magnetometer LIS3mdl is connected(via i2c) to ism330dhcx as an external sensor.

reading magnetometer in power mode = ultra-high mode.

data rate = default

single converstion mode we get a nack saying magnetometer is not responding after 2 hours continuous run.

changed the power mode = lowe power mode and kept remaining same.

now i get MASTER STATUS of ISM330DHCX give NACK after 12 or 15hours of continuous run.

this is the schematics..
_legacyfs_online_stmicro_images_0693W00000dDIoRQAW.pngplease help.. i need to run it continously.

    This topic has been closed for replies.

    2 replies

    Federica Bossi
    ST Technical Moderator
    June 8, 2023

    Hi @Nmaje.1​ ,

    First, looking at your schematic it seems that the magnetomer is connected via SPI and not I2C.

    Referring to the DS at pag 35, for I2C connection between magnetomer and ISM330DHCX you need to connect only MSDA and MSCL.


    _legacyfs_online_stmicro_images_0693W00000dDPW9QAO.pngThen, at pag 37, check the pin status mode2.

    At least, I suggest you to check if CSB_AUX2 is always at high level.

    Let know if this helps.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Nmaje.1
    Nmaje.1Author
    Associate
    June 13, 2023

    @Federica Bossi​ 

    if CSB_AUX2 is high means its i2c communication right!?

    You may choose to use I2C or SPI. 

    Either way, there is external pullup on all lines, specifically both I2C_SDA/SDC and SPI_nCS
    _legacyfs_online_stmicro_images_0693W00000dDgoKQAS.png 

    also I am getting proper data from magnetometer(LIS3MDL) via mode2 as ism330dhcx I2C master. Its just that at times.. my magnetometer stop responding... make the ism330dhcx feel that the external sensor is not responding. will this be because of any incoming extra power ?