Skip to main content
Pritesh Patel
Associate
Jul 17, 2017 6:22 AM UTC
Solved

LIS3MDL BDU

Posted on July 17, 2017 at 08:22

hello,

I have gone through the datasheet and app note of LIS3MDL. But i am not able to get how block data update bit work i.e. if someone has set the BDU bit and if I read registers through I2C one by one, then how the ic internally gets idea that all the registers have been read and got the data of same sample?

Also can anyone please elaborate about ODR and its working in LIS3MDL

This topic has been closed for replies.
Best answer
Jul 17, 2017 4:53 PM UTC
Posted on July 17, 2017 at 18:53

Hello,

Have a look at this application note, available from product webpage:

http://www.st.com/content/ccc/resource/technical/document/application_note/69/d7/05/fe/a9/3e/4b/ea/DM00136626.pdf/files/DM00136626.pdf/jcr:content/translations/en.DM00136626.pdf

. Section 3.2.3 Using the block data update (BDU) feature explains the BDU.

Also ODR is output data rate, how often you can get an updated results. It is declared in Hz, meaning samples per second.

David

11 replies

Best answer
Jul 17, 2017 4:53 PM UTC
Posted on July 17, 2017 at 18:53

Hello,

Have a look at this application note, available from product webpage:

http://www.st.com/content/ccc/resource/technical/document/application_note/69/d7/05/fe/a9/3e/4b/ea/DM00136626.pdf/files/DM00136626.pdf/jcr:content/translations/en.DM00136626.pdf

. Section 3.2.3 Using the block data update (BDU) feature explains the BDU.

Also ODR is output data rate, how often you can get an updated results. It is declared in Hz, meaning samples per second.

David

Pritesh Patel
Associate
Jul 18, 2017 9:16 AM UTC
Posted on July 18, 2017 at 09:16

Hello David,

Thanks for your reply.

But still i am not getting full idea about ODR. So i just want to confirm from you that my understanding is right or not from your answer.   

So what i have understood is, by setting ODR=80Hz, our output registers will be updated every 12.5ms(1/80). Is it right?

ST Employee
Jul 18, 2017 8:01 AM UTC
Posted on July 18, 2017 at 10:01

Yes, your understanding is correct.

Pritesh Patel
Associate
Jul 18, 2017 10:24 AM UTC
Posted on July 18, 2017 at 10:24

Thank You Miroslav for your help.