Skip to main content
lasersocks
Associate
August 28, 2014
Question

LIS3DSH differentiate between State Machine 1 and 2 on INT1 pin

Posted on August 28, 2014 at 16:25

I am using both state machines on the LIS3DSH to analyze two different types of movement. I only have room to use a single INT pin, so I am trying to direct both state machines to it running at the same time.

When the interrupt triggers, is there any way to tell which state machine was the one that triggered the interrupt? I can not find a register that contains a flag showing whether a machine has been triggered.

Thanks for the help!

#lis3dsh
This topic has been closed for replies.

1 reply

lasersocks
Associate
August 28, 2014
Posted on August 28, 2014 at 17:07

Oh dear, I apparently missed the STAT register... answered my own question