Skip to main content
DJi.1
Associate II
December 23, 2019
Question

(LIS3DH) What will be the slave address if the SDO/SA0 neither wired to VSS nor GND?

I have a board that uses LIS3DH. Unfortunately I find the SDO/SA0 pin does NOT wire to VSS or GND. In this case, what would be the Slave ADdress(SAD)?

In the spec it says 001100xb and the 'x' is either 1 or 0 when connected to VSS or GND. But no clue on my case.

Thanks,

This topic has been closed for replies.

8 replies

Piranha
Principal III
December 23, 2019

How about reading pin description in the datasheet?

DJi.1
DJi.1Author
Associate II
December 23, 2019

No content in the datasheet about my case

Piranha
Principal III
December 23, 2019

Table 2. Pin description

7(1)

SDO / SA0

SPI serial data output (SDO) / 2C less significant bit of the device address (SA0)

1. SDO/SA0 pin is internally pulled up. Refer to Table 3 for the internal pull-up values (typ.).

Table 3. Internal pull-up values (typ.) for SDO/SA0 pin

So this is not a content?

DJi.1
DJi.1Author
Associate II
December 23, 2019

Got it. That makes sense. Thanks a lot!​

Piranha
Principal III
December 23, 2019

When connecting SA0 to GND, the current will flow from VDD through internal pull-up to GND. From Table 3.: 3,6 V / 20,4 kOhm = 176 uA. Connecting SA0 to VDD or leaving pin unconnected should be the least current consuming option.

DJi.1
DJi.1Author
Associate II
December 24, 2019

Got it. Thanks a lot.​