Skip to main content
IDEngineer
Associate III
February 12, 2016
Question

LIS3DH: What current ratings for input/output pins?

Posted on February 12, 2016 at 19:38

I've checked the LIS3DH's spec sheet and I can't find specs for input or output current on its I/O pins. Somewhat difficult to design in this part when we don't know its I/O pin current source/sink specs.

Are these documented anywhere? Any data available on this?

Thanks!

#lis3dh-current
This topic has been closed for replies.

1 reply

Simon Wyss
Associate
May 10, 2017
Posted on May 10, 2017 at 23:02

Interesting question!

If one want to use this part in low power application, every uA (and nA) counts.

What are the values of the input (leackage) currents of the SPI and I2C pins?