Skip to main content
Visitor II
April 5, 2024
Question

LIS3DH sensor data offset/value problems

  • April 5, 2024
  • 1 reply
  • 1098 views

We have designed the LIS3DH onto a custom PCBA, and we are seeing some oddities with the sensor readings post manufacturing. The PCBA goes into a two part injection molded enclosure made of ABS, and the two halves are ultrasonically welded together. After this process, we are seeing what appears to be an offset zero issue along two of the axes. The entire range of gravity vectors is as expected at ~18.9m/s^2. However, positive Z facing toward the earth yields a gravity vector magnitude of ~13.8m/s^2 and negative Z down reads ~5.1m/s^2.

Has anyone else seen something like this or have ideas for how to fix this? 

 

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
April 9, 2024

Hi @amk1234321 ,

Welcome to ST Community!

We received your request internally from our region and we have already processed it. They will share all the info with you by tomorrow.

Thanks for your patience :)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.