Skip to main content
RKeit.1
Associate II
April 9, 2020
Question

LIS3DH not responding. Maybe pullup resistor strength or interrupt pin connection.

Hi All,

I have been using the LIS3DH for years and have always found it trouble free.

I have a very small board with an MCU, an Si7051 temperature sensor and an LIS3DH. The two sensors share the same very short I²C bus. There are 10 kΩ pullup resistors on SDA and SCL. The two interrupt pins of the LIS3DH are connected directly to two pins on the MCU. SD0/SA0 is connected directly to ground, a setup I have used before.

The LIS3DH is not responding at all. I can't get an ACK or anything else. I can communicate with the temperature sensor. I have tried bus speeds between 10 kHz and 92 kHz. I have also tried several different configurations for the two MCU pins to which the INT pins are connected. They are open drain inputs.

Could the pullup resistors be too weak? I have used LIS3DH alone with 10 k before but not shared with another device.

Would tying the two INT pins to ground, albiet via a weak pull-down cause the LIS3DH to be unresponsive? I have always found these outputs to be robust. It is just a thought. Should I put a resistor between the each INT pin and the MCU pin? It is a seriously small board and finding space would be hard.

Any clues would be appreciated.

Thanks in advance,

Rob

    This topic has been closed for replies.

    2 replies

    RKeit.1
    RKeit.1Author
    Associate II
    April 9, 2020

    I found the problem. I am dealing with an LIS3DSH, not an LIS3DH. It is all working fine.

    darla14
    Associate III
    November 4, 2020

    what change you spotted which solves the issue.Can you please elaborae. It will help others.