Skip to main content
GTS.1
Associate III
February 10, 2023
Solved

LIS3DH - Issue with using the DREADY interrupt

Hi,

I've tried to configure the DREADY to INT1 and read the output registers. I believe I'm making some mistake in the configuration as I observed that I'm able to read the OUT registers when I using the polling method. I've tried using the ST MEMS C driver and directly writing to the registers. Below is a code snippet of what I tried using to configure the LIS3DH

```

uint8_t lis3dh_on_boot(stmdev_ctx_t *ctx)

{

  uint8_t config[6] = {0x07, 0x00, 0x10, 0xA8, 0x00, 0x01};

  uint8_t config_read[6] = {0};

  uint8_t ctrl_reg0 = 0x90;

  uint8_t ctrl_reg1 = 0x07;

  uint8_t ctrl_reg2 = 0x00;

  uint8_t ctrl_reg3 = 0x80;

  uint8_t ctrl_reg4 = 0xA8;

  uint8_t ctrl_reg5 = 0x00;

  uint8_t ctrl_reg6 = 0x02;

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG0, &ctrl_reg0, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG1, &ctrl_reg1, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG2, &ctrl_reg2, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG3, &ctrl_reg3, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG4, &ctrl_reg4, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG5, &ctrl_reg5, 1);

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG6, &ctrl_reg6, 1);

  nrf_delay_ms(50);

  ctrl_reg1 = 0x17;

  lis3dh_write_reg(ctx, LIS3DH_CTRL_REG1, &ctrl_reg1, 1);

  nrf_delay_ms(50);

  lis3dh_read_reg(ctx, LIS3DH_CTRL_REG1|0x80, config_read, 6);

  lis3dh_read_reg(ctx, LIS3DH_CTRL_REG0, &ctrl_reg0, 1);

}

```

I believe the code to configure the interrupt pins is fine as the pin stayed high when I tried to read it.

This topic has been closed for replies.
GTS.1
GTS.1Best answer
Associate III
February 16, 2023

Figured out the issue in the above code. The value I used for CTRL_REG3 is incorrect. I think the C driver didn't work initially as the interrupt was latched and I hadn't added in the code to read the output registers. So the interrupt stayed latch and it did not trigger the ISR.

2 replies

GTS.1
GTS.1AuthorBest answer
Associate III
February 16, 2023

Figured out the issue in the above code. The value I used for CTRL_REG3 is incorrect. I think the C driver didn't work initially as the interrupt was latched and I hadn't added in the code to read the output registers. So the interrupt stayed latch and it did not trigger the ISR.

Eleon BORLINI
ST Employee
February 16, 2023

Thank you @GTS.1​  for sharing your solution!

-Eleon