Skip to main content
josescxavier
Associate II
Oct 18, 2019 2:07 PM UTC
Question

LIS3DH Interrupt line

Hi,

Is it possible to disable the interrupt line? By default it is Default: push-pull output forced to GND but I would like to be able to make it floating to use the ucontroller gpio connected to INT1 for other purposes like UART TX.

Thank you

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
Oct 21, 2019 9:05 AM UTC

Hi @josescxavier​ , do you mean change the INT1 internal config from push-pull to open-drain? Unfortunately is not possible... please note that even if the pull down to gnd is very weak, the use of INT1 pin routed to UART com could cause a little x-talk. Better to leave it unconnected, even if I suspect it would require a HW rework. Regards