Skip to main content
rihana
Visitor II
June 7, 2015
Question

LIS3DH INT2 Configuration

Posted on June 07, 2015 at 19:15

Hi,

For LIS3DH, the datasheet mentions two user programmable interrupts INT1 and INT2. Though config, threshold, duration etc. (INT1_CFG, INT1_SRC, INT1_THS, INT1_DURATION) registers are listed for INT1, no such registers for INT2 was listed in the register mappings. Is INT2 configuration and  functionality different from that of INT1? This was not clear to me from the datasheet or application note of LIS3DH. Please help.

Thanks,

Rihana

#lis3dh #interrupt #int2
This topic has been closed for replies.

3 replies

rslima
Visitor II
August 13, 2015
Posted on August 13, 2015 at 20:02

Hello,

I am exactly with the same doubt.

Rihana did you get any answer?

rvalle
Associate
March 17, 2016
Posted on March 17, 2016 at 06:42

Mee to.

I want to detect both changes in orientation plus freefall. Wich is said to be supported.

Yet, how do you setup INT2?

ST??

argo777
Visitor II
March 29, 2016
Posted on March 29, 2016 at 12:20

Exactly same situation!!!!