Skip to main content
alzaabi401
Visitor II
November 16, 2014
Question

LIS3DH inertial interrupt/wake-up not detected

  • November 16, 2014
  • 2 replies
  • 1049 views
Posted on November 16, 2014 at 23:55

I am unable to detect an interial interrupt from the LIS3DH accelerometer as a result of moving the sensor on a flat surface. The sensor is interfaced with an Arduino Uno using I2C. I am using the example in section 6.3.1 of AN3308, LIS3DH application notes. I can successfully read acceleration values. I also tried checking both interrupt ports, int 1 and int 2.

Please see attached Arduino code below.

&sharpinclude <Wire.h>

const int LIS3DH_ADDR = 0x18;

int pin = 13;

int int1Pin = 2;

int int2Pin = 3;

/* I2C Communication Set-up ---------------------------------------------------------*/

unsigned int readRegister(byte reg) {

  Wire.beginTransmission(LIS3DH_ADDR);

  Wire.write(reg);

  Wire.endTransmission();

  

  Wire.requestFrom(LIS3DH_ADDR, 1);

  return Wire.read();

}

void writeRegister(byte reg, byte data) {

  Wire.beginTransmission(LIS3DH_ADDR);

  Wire.write(reg);

  Wire.write(data);

  Wire.endTransmission();

}

/* Initialize accelerometer in the host processor. ----------------------------------*/

//It only needs to be executed one time after power up in initialization routine.

void init_ACC(void)

{

    // configurations for control registers

    writeRegister(0x20, 0xA7); //Write A7h into CTRL_REG1;      // Turn on the sensor with ODR = 100Hz normal mode.

    writeRegister(0x21, 0x00); //Write 00h into CTRL_REG2;      // High-pass filter (HPF) disabled 

    writeRegister(0x22, 0x40); //Write 40h into CTRL_REG3;      // ACC AOI1 interrupt signal is routed to INT1 pin.

    writeRegister(0x23, 0x00); //Write 00h into CTRL_REG4;      // Full Scale = +/-2 g

    writeRegister(0x24, 0x00); //Write 00h into CTRL_REG5;      // Default value. Interrupt signals on INT1 pin is not latched. 

                                                                //Users don�t need to read the INT1_SRC register to clear the interrupt signal.

    // configurations for wakeup and motionless detection

    writeRegister(0x32, 0x10); //Write 10h into INT1_THS;          // Threshold (THS) = 16LSBs * 15.625mg/LSB = 250mg.

    writeRegister(0x33, 0x00); //Write 33h into INT1_DURATION;     // Duration = 1LSBs * (1/10Hz) = 0.1s.

    writeRegister(0x30, 0x0A); //Write 0Ah into INT1_CFG;          // Enable XLIE, YLIE interrupt generation, OR logic.

 

}

void setup() {

  Wire.begin();

  Serial.begin(9600);

  int res = readRegister(0x0F); //WHO_AM_I

  Serial.println(res);

  pinMode(pin, OUTPUT);      // sets the digital pin 13 as output

  pinMode(int1Pin, INPUT);      // sets the digital pin 2 as input

  pinMode(int2Pin, INPUT);      // sets the digital pin 2 as input

}

void loop() {

  //Read both interrupt pins

  int int1 = digitalRead(int1Pin);

  int int2 = digitalRead(int2Pin);

  Serial.print(int1);

  Serial.print('','');

  Serial.println(int2);

  

 if (digitalRead(int1Pin) == 0 && digitalRead(int2Pin) == 0){

   //if both are low write

   writeRegister(0x30, 0x0A);

 }

 else {

   digitalWrite(pin, HIGH);

   int intEvent = readRegister(0x31);

   Serial.println(intEvent);

   delay(2000);

 }

   

delay(0);

}

#lis3dh-interrupt #accelerometer #lis3dh #lis3dh-interrupt
This topic has been closed for replies.

2 replies

zhang_qiang_up
Visitor II
March 2, 2015
Posted on March 02, 2015 at 10:25

I am be able to read out the x y z raw data from the acc lis3dh.

But I it can not generate INT signal. There is my configuration of the acc.

      LIS3DH_WriteReg(LIS3DH_CTRL_REG1,0x27);

 

      LIS3DH_WriteReg(LIS3DH_CTRL_REG2,0x01);

      // Interrupt driven to INT1 pad,  AOI1 interrupt on INT1.  ---0100

      LIS3DH_WriteReg(LIS3DH_CTRL_REG3,0x40);

      // FS = 2g  Full scale selection 

      LIS3DH_WriteReg(LIS3DH_CTRL_REG4,0x00);

     // Disable FIFO temporarily;  0: interrupt request not latched;---0x00

     //latched  0000 1000 ---0x08

      LIS3DH_WriteReg(LIS3DH_CTRL_REG5,0x08);  

     LIS3DH_WriteReg(LIS3DH_INT1_THS,0x08); 

    // 0010 1010 beyond thresh hold  ; 0001 0101  below thresh hold. event

      LIS3DH_WriteReg(LIS3DH_INT1_CFG,0x2a);

      uint8 val;

      LIS3DH_ReadReg(0x31, &val);    //INT1_SRC

------

When I shake the acc, it just not generate INT signal , INT1 pin is low.

zhang_qiang_up
Visitor II
March 3, 2015
Posted on March 03, 2015 at 10:21

Problem Found.

!!! without the delays between I2C operations, ACC is not configured correctly!!!

Add delays. It works. MCU is Dialog M0.