Skip to main content
Mich1
Associate III
December 16, 2013
Question

LIS3DH datasheet error?

Posted on December 16, 2013 at 14:53

In LIS3DH datasheet (Doc ID 17530)

on table 25 we can see: Default value 00     ODR3-0 (0000:50Hz Others:...)

on table 26 we can see: 0000 Power down mode

So what is ODR = 0000  Power down or 50Hz?

#lis3dh
This topic has been closed for replies.

1 reply

bw_it
Associate
February 19, 2014
Posted on February 19, 2014 at 12:09

Hi,

ODR = 0000 is power down, this is confirmed in Applicaiton note AN3308.

My experience is that the application notes are the most reason updated.