Skip to main content
jose
Visitor II
March 25, 2014
Question

LIS3DH Click Interrupt

Posted on March 25, 2014 at 22:50

The data sheet makes no explicit mention of a way to force this interrupt to latch and clear when the CLICK_SRC register is read (like the INT1_CFG registers can).

App note AN3308 states that this behavior can be achieved by setting the LIR bit in the TAP_CFG register.  However, this bit is not documented in the data sheet.  Another, similar part perhaps?

I'm seeing the interrupt hold for the duration of the CLICK_LATENCY period as expected but would like to clear this sooner as I'm using the data ready signal on the same line.  Is there anything I can do to accomplish this?  I'm sampling at a fairly low data rate (10hz) so shortening the latency period is not an option.  I am using an OEM board that does not have INT2 hooked up.

#li3dh-click
This topic has been closed for replies.

1 reply

Taylor.Sean
Associate III
July 15, 2014
Posted on July 15, 2014 at 16:42

Any updates on this ?  I am having the same problem.  The click activates the external interrupt line, but reading CLICK_SRC register doesn't give any information on the source of the interrupt.