Skip to main content
Daniel S.
Associate II
June 22, 2017
Question

LIS331HH, understanding self test

Posted on June 22, 2017 at 14:51

We have two prototype boards each equipped with a LIS331HH.

One of the sensors seems completely broken because the Z axis shows values around 2.3g while laying flat on the table. Because of that we were now looking into self tests to check all sensors in production.

We query all the axis and divide each value by 16. The data sheet tells us that 1digit is 3mg so we expect 333 on the Z axis and 0 on X and Y. We measure X:20, Y: 35 and Z: 373, which is an offset we expect [1].

Now we start the self test in plus mode and measure X: 177, Y: 131 and Z: 828.

The self test values differ by X: 157, Y: 96 and Z: 455 from the non self test values.

In the data sheet there are values for 'self-test output change'. Those mean, that X and Y are supposed to differ by a max of 180 and that Z may only differ by 370?

So this sensor passes the test on X and Y and fails on Z and therefore we have to throw this sensor away, right? Or did we misunderstand the process and did it wrong?

Thanks in advance

Daniel

[1] 

https://community.st.com/0D50X00009XkghXSAR

 

null
    This topic has been closed for replies.

    1 reply

    ST Employee
    June 22, 2017
    Posted on June 22, 2017 at 15:21

    Yes, your understanding is completely correct.

    Self-test output change in Z axis should be 220-370 LSB, if the output is 455 the sensor is broken.