Skip to main content
SVozl.1
Associate
May 10, 2022
Question

LIS331HH self-test output change with voltage

We have performed the self test on two prototype boards,

as instructed in this post: https://community.st.com/s/question/0D50X00009XkXegSAF/lis331hh-understanding-self-test

The x and y differences are around 135, which is in the range, but on the z axis we get around 380, which according to the datasheet, is just enough to no pass the self test.

The datasheet also specifies that the "Self-test output changes with the power supply" and that the product was calibrated at 2.5V.

Our question is the following:

Can the fact that we use a different supply voltage (3.3V) be the reason why the self test (just barely) fails or does the range of the self test already account for potencial differences?

Best regards!

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    May 10, 2022

    Hi @Sašo Vozli�?​ ,

    are both the prototype boards failing the self test?

    And did you follow the self test procedure as suggested on the C drivers on Github --> lis331dlh_self_test.c?

    The Vdd could slightly impact the data on this product, but should not make the difference between pass and fail. Please be sure to be in a controlled environment during the self test.

    -Eleon

    SVozl.1
    SVozl.1Author
    Associate
    May 11, 2022

    Hi Eleon,

    yes, both are failing the self test. We'll try to run a test with 2.5V instead of 3.3V.

    We did follow the procedure.

    On a related note, how does a negative self test sign impact the results?

    Do we just change the sign on the specified ranges?

    Do we have to run the self test in both directions?

    PS: If the self test fails with the positive sign, but passed with the negative one, how do we interpert that?

    Best regards,

    Sašo