Skip to main content
bosquet
Visitor II
February 5, 2015
Question

LIS331DLH problem value

Posted on February 05, 2015 at 09:01

.ExternalClass8B0DBA798B5B4AA8BE4D83498BC56468 p {margin-bottom:0.25cm;line-height:120%;} .ExternalClass8B0DBA798B5B4AA8BE4D83498BC56468 a:link {;}

Hello,

I use the accelerometer LIS331DLH but I have a problem about values.

The MEMS is conect to the card Mbed FRDM-K64F, 3,3V supply and SPI bus communication.

I use this datasheet :

http://www.st.com/web/en/resource/technical/document/datasheet/CD00213470.pdf

and this application note

http://www.st.com/web/en/resource/technical/document/application_note/CD00215823.pdf

Communication is OK, WHO_I_AM returns 0x32.

In my program, I follow the Start-up sequence and reading data sequence write in application note.

spiWriteByte(0x20,0x27,cs); // CTRL_REG1 0x20

spiWriteByte(0x20,0x27,cs);

spiWriteByte(0x21,0x00,cs); // CTRL_REG2 0x21

spiWriteByte(0x22,0x00,cs); // CTRL_REG3 0x22

spiWriteByte(0x23,0x00,cs); // CTRL_REG4 0x23

spiWriteByte(0x26,0x10,cs); // REFERENCE 0x26

spiWriteByte(0x32,0x00,cs); // INT1_THS 0x32

spiWriteByte(0x33,0x00,cs); // INT1_DUR 0x33

spiWriteByte(0x36,0x00,cs); // INT2_THS 0x36

spiWriteByte(0x37,0x00,cs); // INT2_DUR 0x37

uint8_t regHP_FILTER=spiReadByte(0x25,cs); //read HP_FILTER_RESET (if filter is enabled)

spiWriteByte(0x30,0x00,cs); // INT1_CFG 0x30

spiWriteByte(0x34,0x00,cs); // INT2_CFG 0x34

spiWriteByte(0x24,0x00,cs); // CTRL_REG5 0x24

My problem is that values returns is false

1g, I have :

X_H= 0x00 X_H= 0x40

Y_H=0x00 Y_H=0x10

Z_H=0x13 Z_H=0x20

And applicatin note write :

X_H= 0x00 X_H= 0x00

Y_H=0x00 Y_H=0x00

Z_H=0x40 Z_H=0x00

-1g, I have :

X_H= 0x00 X_H= 0x40

Y_H=0x00 Y_H=0x10

Z_H=0xe9 Z_H=0x20

And applicatin note write :

X_H= 0x00 X_H= 0x00

Y_H=0x00 Y_H=0x00

Z_H=0xC0 Z_H=0x00

Also I must write 2 times in CTRL_REG1 registry to change the mode to ''Normal-mode''

Can you explain to me my mistake.

#lis331dlh
This topic has been closed for replies.