Question
LIS331DL SPI communication issue
- 2 replies
- 1179 views
Hi guys,
I met a SPI communication issue about LIS331DL. The type of kit board is MKI153. When I tied VDDIO and VDD to 3.3V, the data from chip register by SPI isn't correct. When I only connect VDD to 3.3v, The data is correct.
The register is WHO_AM_I and CTRL_REG1.
Tie vddio and vdd together: WHO_AM_I register value = 0x20 CTRL_REG1 = 0x06
In this case: vddio & vdd = 3.3v
Only connect VDD: WHO_AM_I register value = 0x32 CTRL_REG1 = 0x07
In this case: vdd = 3.3v. vddio is around 2.5v (vddio pin is floating)
Pls see attached pictures. I can't understand this issue. Could you check it?
Thanks!