Skip to main content
Associate II
Apr 27, 2026 2:11 PM UTC
Question

LIS2MDL magnetometer with steval_mki181v1

Hello everyone,

I'm working with the LIS2MDL sensor (steval_mki181v1) , i made a connection between it and the nrf5340 and I configured it over I2C with pull-up resistors enabled.

-VDD -- > VDD

-VDDio --> VDD

-CS --> VDD 

-PIN I2C  :: SCL to SCL et SDA to SDA

-GND t GND

Current configuration:

  • I2C communication working (i got the chip id 0x40)

  • Block Data Update (BDU) enabled

  • Output Data Rate tested at 10 Hz or50 Hz

  • Offset cancellation enabled

  • Continuous mode enabled

  • I applied the offset XYZ as :: 
    int16_t mag_offset[3] = {
    0xF500, /* OFFSET_X_REG */
    0xF800, /* OFFSET_Y_REG */
    0xF400, /* OFFSET_Z_REG */
    };

However, I noticed that the values I read from the sensor remain almost always the same and do not update as expected, as shown in the photo below.

Could anyone help me understand what might be causing this issue or guide me on how to troubleshoot it?

Any help would be greatly appreciated. Thank you!

ASREB_0-1777298804785.pngASREB_1-1777298856405.png

 

17 replies

ASREBAuthor
Associate II
May 11, 2026 11:37 AM UTC

Hello I need  a response please can u help me ?? 

 

Associate III
May 11, 2026 12:12 PM UTC

They do not reply to all questions, sometimes you are in the field of knowledge on your own.  

How are you using the device.  It can be read with a C# program quite nicely, but that depends on the use

Associate III
May 11, 2026 12:11 PM UTC

Are you using the 109 board to handle the communication?  

ASREBAuthor
Associate II
May 11, 2026 12:14 PM UTC

Thank u for your response ....

i used c programmin , i used the board nrf5340 (nordic board) et le lis2mdl dans le module steval_mki181v1

Andrew Neil
Super User
May 18, 2026 3:19 PM UTC

@ASREB wrote:

i used the board nrf5340 (nordic board) et le lis2mdl dans le module steval_mki181v1


Have you tried using an ST board, and ST's provided software ?

Obviously, issues with the nRF5340 are beyond the scope of this forum - so would be good to remove that as an "unknown".

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 18, 2026 2:43 PM UTC

I need a response , can u help me ST community?? 

Andrew Neil
Super User
May 18, 2026 3:16 PM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

A schematic is more useful than a text list of connections.

 


@ASREB wrote:

i made a connection between it and the nrf5340 and I configured it over I2C with pull-up resistors enabled.


What pullups did you use?

Have you used an oscilloscope to verify that you have good, clean edges?

See the diagram here for the effects of pullup resistance - from too low to too high ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 18, 2026 3:24 PM UTC

Hello Andrew
I don’t think the problem comes from the Zephyr driver, because the driver uses the same logic as the ST driver, especially in this configuration.

https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2mdl_STdC/examples/lis2mdl_read_data_polling.c

Andrew Neil
Super User
May 18, 2026 3:38 PM UTC

Have you actually tried that example?

You didn't answer about the pullups, or schematic.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 18, 2026 3:49 PM UTC

yes i tried this example with the same configuration. 

About this "You didn't answer about the pullups, or schematic." yes i added the pullpus for i2c , what about schematic ?? 

Andrew Neil
Super User
May 18, 2026 4:07 PM UTC

I asked what pullups did you use - what value?

 


@ASREB wrote:

yes i tried this example with the same configuration. 


And did it work?

 


@ASREB wrote:

what about schematic ?? 


Post it!

 

You moan about people not answering, but then don't provide information asked for.

 How to write your question to maximize your chances to find a solution 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 18, 2026 4:13 PM UTC

i used steval-mki181v1 (with lis2mdl sensor)with this schematic ::

VDD -- > VDD

-VDDio --> VDD

-CS --> VDD

-PIN I2C :: SCL to SCL et SDA to SDA

-GND t GND

About the configuration , yes the sensor response with XYZ data but they stay the same data ( but in the configuration i put continuous mode and not single shot).

 

ASREB_0-1779120800841.png

 

Andrew Neil
Super User
May 18, 2026 4:28 PM UTC

That's not a schematic - that's just a text list.

Again, a schematic is a far better way to convey this information.

You still haven't said what pullups did you use - what value ?

 


@ASREB wrote:

the sensor response with XYZ data but they stay the same data 


Is that using the ST example ?

What changed do you thing should happen in the data? 

How are you forcing those changes?

 

Remember that we know nothing about you, your project, or your setup - it is entirely up to you to provide clear and complete descriptions.

Again, please see:  How to write your question to maximize your chances to find a solution 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 18, 2026 4:53 PM UTC

ASREB_0-1779122789980.png

ASREB_1-1779122997086.png

 

About the pull-up, I enabled the software pull-up.
Regarding the schematic, you can also find the related figure attached.

For the ST example, I didn’t make any modifications. I simply used the same configuration and then read the XYZ data. However, the data is always repeated, as shown in the figure.

One thing I noticed is that if I reboot the board sometimes (power off/on), I get new data values, but then those values remain repeated again until the next reboot.

I hope my response clear.

Thanks a lot for your help.

I appreciate your efforts.

Andrew Neil
Super User
May 18, 2026 5:14 PM UTC

@ASREB wrote:

About the pull-up, I enabled the software pull-up..


You mean the internal pullups - inside the STM32 or the nRF ?

These are unlikely to be suitable for I2C - their value is too high.

Again, have you looked with a scope to verify that you have good signals on the I2C wires?

 


@ASREB wrote:

the data is always repeated, as shown in the figure..


Again, what are you doing that would make it change ?

Have you used a logic analyser to see what's actually happening on the wires ?

ie, is the sensor itself sending constant data, or is your software just ignoring updates ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ASREBAuthor
Associate II
May 19, 2026 2:19 PM UTC

Hello, 

I checked I2C and another fature....
I found the issue but I don't fully understand how to resolve. Just to more explain u, I am working with an nRF5340 board and the LIS2MDL sensor. When I reboot the board to retrieve the X, Y, and Z magnetic values, I always get exactly the same values, even after rebooting multiple times. While investigating the problem further, I noticed something strange: when I disconnect the UART pins, the values li2mdl change. Each time I connect or disconnect the UART pins, the sensor values update.

Andrew Neil
Super User
May 19, 2026 2:31 PM UTC

You still haven't said what pullups you're using !

As noted, correct pullups are critical to correct & reliable operation of I2C.

 

Do you see the same behaviour on an ST board ?

How, exactly, do you "connect the UART pins" ?

 

Bizarre behaviour like this is often due to poor connections; particularly poor GND and/or VDD connections - see this post.

Again, have you used an oscilloscope to see what's actually happening on the wires?

 

PS:

The  X-NUCLEO-IKS4A1 features an LIS2MDL

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.