Skip to main content
Associate II
February 8, 2024
Solved

LIS2MDL Magnetometer unable to find vdd supply

Hi 

I am using the LIS2MDL Magnetometer, which is connected to i2c0 on my custom board. I have enabled the respective kernel configuration for the magnetometer.

CONFIG_IIO_ST_SENSORS_I2C=y
CONFIG_IIO_ST_SENSORS_SPI=y
CONFIG_IIO_ST_SENSORS_CORE=y

CONFIG_IIO_ST_MAGN_3AXIS=y
CONFIG_IIO_ST_MAGN_I2C_3AXIS=y
CONFIG_IIO_ST_MAGN_SPI_3AXIS=y
 

The implemented device tree is provided below.

\{

regulator_1: regulator-1 {
compatible = "regulator-fixed";
regulator-name = "regulator.1";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};

};

&i2c0 {
status = "okay";
lis2mdl: lis2mdl@1e {
compatible = "st,lis2mdl";
reg = <0x1e>;
vdd-supply = <&regulator_1>;
vddio-supply = <&regulator_1>;
};
};

When my board booted up, I checked whether the driver was probed or not. However, it did not get probed. I have attached my dmesg log below.

 

[ 4.624377] st-magn-i2c 0-001e: supply vdd not found, using dummy regulator
[ 4.631410] st-magn-i2c 0-001e: supply vddio not found, using dummy regulator
[ 4.638715] iio iio:device3: DRDY on pdata not valid.
[ 4.643880] st-magn-i2c: probe of 0-001e failed with error -22
[ 4.649725] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 38

The hardware connections that we checked are fine, but I don't know why this error is happening. Can anyone kindly assist me in debugging this issue?

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
February 9, 2024

Hi @Perumalsamy ,

Can you try to use our official drivers and let me know if the problem persists?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
February 9, 2024

Hi @Perumalsamy ,

Can you try to use our official drivers and let me know if the problem persists?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
February 9, 2024

Thank You @Federica Bossi