Skip to main content
Associate II
January 14, 2024
Question

LIS2MDL Magnetometer Probe failed and Vdd power supply not found, dummy regulator issue

Hi,

I have successfully connected the LIS2MDL magnetometer to my reference board via I2C, and it is detected. However, after enabling the necessary kernel configurations and device tree, it indicates that the VDD supply is not found, and it resorts to using a dummy regulator supply. Additionally, there is a probing issue. I have provided the enabled configurations, device tree, and logs below.

kernel configuration

CONFIG_IIO_ST_SENSORS_I2C=y
CONFIG_IIO_ST_SENSORS_SPI=y
CONFIG_IIO_ST_SENSORS_CORE=y

CONFIG_IIO_ST_MAGN_3AXIS=y
CONFIG_IIO_ST_MAGN_I2C_3AXIS=y
CONFIG_IIO_ST_MAGN_SPI_3AXIS=y

device tree

&i2c0 {
status = "okay";

lis2mdl: lis2mdl@1e {
compatible = "st,lis2mdl";
reg = <0x1e>;
vdd-supply = <&reg_3v3>;
vddio-supply = <&reg_3v3>;
};

regulators {
reg_3v3: regulator-3v3 {
compatible = "regulator-fixed";
regulator-name = "3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
};

boot log

[ 3.681279] st-magn-i2c 0-001e: supply vdd not found, using dummy regulator
[ 3.693564] st-magn-i2c 0-001e: supply vddio not found, using dummy regulator
[ 3.728755] st-magn-i2c: probe of 0-001e failed with error -22

Can I make any changes to the device tree or kernel configuration? Could someone kindly assist me in resolving this issue?

 

  

This topic has been closed for replies.

8 replies

Federica Bossi
ST Technical Moderator
January 18, 2024

Hi @Perumalsamy ,

 

I can support you only if something related to the hardware, can you share your schematic?

Unfortunately, in case your issue is related to your own firmware we can't support you because it's not an ST product.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
January 18, 2024

I think this is ST product
https://www.st.com/resource/en/datasheet/lis2mdl.pdf

I connected the sensor in the i2c bus of zcu106 Evaluation Board.

https://www.mouser.com/datasheet/2/903/ug1244-zcu106-eval-bd-1596082.pdf#page=122&zoom=100,122,349

I add my connection flow in the below document for your kind reference

Federica Bossi
ST Technical Moderator
February 1, 2024

Hi @Perumalsamy ,

From your schematic I don't see CS, SDO and VDDIO. How are they connected?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
February 1, 2024

I am connected these pins in the i2c. I need only these pins 3v3, GND, SDA and SCL. If the above mentioned pins are need to be connected, kindly assist me.

Federica Bossi
ST Technical Moderator
February 5, 2024

Hi @Perumalsamy ,

Yes, if you don't connect CS, SDO and VDDIO it will not work. Please, follow our guideline and connect them.

For the drivers you find those on our github.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
February 6, 2024

Hi @Federica Bossi 

Thank you for your help. Is there any changes I need to done on the device tree part. Can you give me a example device tree for LIS2MDL Magnetometer.