Skip to main content
Associate II
October 12, 2024
Question

LIS2DW12 wake up interrupt on int1 pin

Hello,

I have an issue related to LIS2DW12 wake up interrupt. When reading the wake interrupt src it is showing that wake up interrupt is being triggered I am getting value in loop from software interrupt. But after enabling interrupt on INT1 pin I am not getting interrupt over INT1 pin. It's being kept at 0.00 volts. Below is my code snippet (controller I am using is NRF52832):

uint32_t app_mpu_init(void) //LIS2DW12 INIT LOGIC
{
    uint32_t err_code;
    uint8_t data;
    // Initate TWI or SPI driver dependent on what is defined from the project
    err_code = nrf_drv_mpu_init();
    if(err_code != NRF_SUCCESS) return err_code;
   
    data = readRegister(LIS2DW12_WHO_AM_I);
    NRF_LOG_INFO("0X%02X ", data); //Getting 0x44 which is correct
 
    err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL2, 0x40);
    if(err_code != NRF_SUCCESS) return err_code;
    nrf_delay_ms(1);
    err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL2, 0x80);
    if(err_code != NRF_SUCCESS) return err_code;
    nrf_delay_ms(25);
 
    err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL1, 0x30);
    if(err_code != NRF_SUCCESS) return err_code;
 
    err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL3, 0x00);
    if(err_code != NRF_SUCCESS) return err_code;
 
    err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL6, 0x0C);
    if(err_code != NRF_SUCCESS) return err_code;
 
    return NRF_SUCCESS;
}

Below is the interrupt enable logic:

uint32_t app_mpu_int_enable(void) // Enabling interrupt on LIS2DW12 IC
{
  uint32_t err_code;
 
  err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL_REG7, 0x00);
  if(err_code != NRF_SUCCESS) return err_code;
  nrf_delay_ms(1);
 
  err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL4_INT1_PAD_CTRL, 0x20);
  if(err_code != NRF_SUCCESS) return err_code;
 
  err_code = nrf_drv_mpu_write_single_register(LIS2DW12_WAKE_UP_DUR, 0x00);
  if(err_code != NRF_SUCCESS) return err_code;
 
  err_code = nrf_drv_mpu_write_single_register(LIS2DW12_WAKE_UP_THS, 0x42);
  if(err_code != NRF_SUCCESS) return err_code;
 
  err_code = nrf_drv_mpu_write_single_register(LIS2DW12_CTRL_REG7, 0x60);
  if(err_code != NRF_SUCCESS) return err_code;
 
  return NRF_SUCCESS;
}
Need help in getting interrupt over INT1 pin checked with oscilloscope not interrupt is being routed to INT1 pin.
Please let me know if any further information you require. Our product is in final stage and we have a huge qty of 10k by this first quarter of 2025.

This topic has been closed for replies.

3 replies

yashg25Author
Associate II
October 14, 2024

Hello, waiting for response

Federica Bossi
ST Technical Moderator
October 23, 2024

Hi @yashg25 ,

Did you try to follow our example on Github?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yashg25Author
Associate II
October 23, 2024

Hi @Federica Bossi 

I have tried the following example but still I am not getting any interrupt over INT1 pin.