Associate
July 19, 2024
Solved
LIS2DW12 Unable to communicate through I2C
- 3 replies
- 1522 views
Hi,
I am using the LIS2DW12 on my board communicating over I2C with the nRF52840. I have not yet been able to communicate with the accelerometer at all, and all attempts to read or write end the same way (see screenshot)
I have the CS and SA0 lines both pulled up to VDD, and VDDIO is tied to VDD because they are the same voltage, 1.8V. Could there be an issue with VDD and VDDIO being the same rail?