Skip to main content
Chiku
Associate II
April 16, 2022
Question

LIS2DW12 in STEVAL-Smartag1 showing only 1024mg value when it is steady, What it means?

  • April 16, 2022
  • 4 replies
  • 1285 views

..

    This topic has been closed for replies.

    4 replies

    Chiku
    ChikuAuthor
    Associate II
    April 16, 2022

    I am using STEVAL-SMARTAG1 anf NFC Phone,

    With the help of App ST NFC Sensor app.. i only can read 1024 mg acceleration/min.

    What does this means? can you explain how mg is related with Acceleration?

    Eleon BORLINI
    ST Employee
    April 19, 2022

    Hi @Chiku​ ,

    Which acceleration axis are you reading? Or are you reading the 3 dimensional acceleration module?

    Consider that the LIS2DW12 accelerometer is 3 axial device, and in a rest condition with Z axis pointing to the ceiling and X and Y on the plane, the output will be about 1g (1000mg) for the Z axis that is measuring the Earth gravity acceleration, and about 0mg for both X and Y axes.

    In case you are reading the total acceleration module, the results will be similar, since it is just the vectoral sum of the 3 above mentioned components.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

    -Eleon

    Chiku
    ChikuAuthor
    Associate II
    April 19, 2022

    Thanks Eleon.

    Sometime i could read 3014 mg when i placed from one location to another.

    How acceleration it calculated? can you brief one example (Sorry for Dumb question but i am new for this)

    Eleon BORLINI
    ST Employee
    April 22, 2022

    Hi @Chiku​ ,

    in this case you are probably moving the board and you are reading the consequent linear acceleration.

    -Eleon