Skip to main content
echt
Associate
October 30, 2017
Solved

LIS2DW12, how are the interrupt pins internally connected?

Posted on October 30, 2017 at 10:02

LIS2DW12, if interrupt pins (INT1 & INT2) are configured to open-drain mode, will they still work if the VDDIO supply is cutoff? (and the interrupt pins are pulled up to another supply voltage) and the VDD is still connected to 1,8V ? Will the VDD voltage still control the open-drain pins or is it completely fed by the VDDIO voltage?

#lis2dw12
This topic has been closed for replies.
Miroslav BATEKBest answer
ST Employee
October 30, 2017
Posted on October 30, 2017 at 10:11

The control logic is powered from the VDDIO so the interrupts will not work if the VDDIO won't be connected.

I don't see a reason why would you do that. Usually the VDDIO remains connected and the VDD is switch on/off to reduce the power consumption.

2 replies

Miroslav BATEKBest answer
ST Employee
October 30, 2017
Posted on October 30, 2017 at 10:11

The control logic is powered from the VDDIO so the interrupts will not work if the VDDIO won't be connected.

I don't see a reason why would you do that. Usually the VDDIO remains connected and the VDD is switch on/off to reduce the power consumption.

echt
echtAuthor
Associate
October 30, 2017
Posted on October 30, 2017 at 10:44

In our application, we would like to leave the LIS2DW12 always on in some lowpower mode. I thought we still would have some leakage on the VDDIO side of things. But the internal pull-ups are on pins we don't use. 

Thanks for the quick response. My question is answered.