Skip to main content
Visitor II
Jun 12, 2025 11:18 AM UTC
Solved

LIS2DW12 – Detecting Orientation Change in Degrees Using Interrupt

We are using the LIS2DW12 accelerometer in our custom product. We understand that this sensor can detect movement or positioning along the X, Y, and Z axis. However, in our application, we need to detect when the device changes its orientation in terms of degrees—for example, when it flips or tilts significantly from one position to another.

Can the LIS2DW12 generate an interrupt based on such orientation changes (e.g., using 6D orientation detection)? We are looking for a way to trigger events when the device is rotated beyond a certain angle.

Thank you

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jun 12, 2025 1:57 PM UTC

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jun 12, 2025 1:57 PM UTC

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.