Skip to main content
Msaga.1
Associate III
Jun 29, 2021 11:23 AM UTC
Solved

lis2dw12 continues mode

Hi I want to use the continues mode feature, so I can read and write from the buffer simultaneously. I have trued to find an example, do you have anything that help?

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Jul 1, 2021 1:12 PM UTC

Hi @Msaga.1​ ,

I see you posted this question, can we refer to that one?

-Eleon

3 replies

Eleon BORLINI
ST Employee
Jun 29, 2021 1:39 PM UTC

Hi @Msaga.1​ ,

did you already check the C example on Github that implements the FIFO mode for the LIS2DW12? --> lis2dw12_read_fifo.c

Starting from this example, and referring to the AN5038 application note at p.39:

Follow these steps for FIFO Continuous configuration which sets a threshold to generate an interrupt to trigger a read by the application processor:

1. Set FTH[4:0] to 31 #watermark level at full scale

2. Set INT1_FTH to ‘1’ #enable FIFO threshold interrupt

3. Activate Continuous mode by setting the FMode[2:0] field to 110b in the FIFO_CTRL register (2Eh) #when the FTH interrupt is generated, data is read from the accelerometer output registers.

Can this operating mode fit your target application?

-Eleon

Msaga.1
Msaga.1Author
Associate III
Jun 30, 2021 8:07 AM UTC

yes i did this , however will this enable me to read and write from the accelerometer buffer at the same time?

for example - I want to be able to read before the buffer is full ( so less then 32 samples) and at the same time the next samples will be writen.

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Jul 1, 2021 1:12 PM UTC

Hi @Msaga.1​ ,

I see you posted this question, can we refer to that one?

-Eleon